This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

capt_basic_continuous

Overview

This example shows how to capture touch data using CAPT continuous mode. CAP polls and samples the touch pad data round by round, in each round, all the enabled pins are sampled one by one. To monitor one pad sample finished, both the yes_touch and no_touch interrupt is enabled. The poll done interrupt is enabled to monitor the poll round finished. The delay period between two polling round is configurable, in this example, the delay period is set to about 0.5s. When the example runs, the sampled data is shown in the terminal, and update every about 0.5s. When electrode plate is touched, the sampled data changes too.

Supported Boards