This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

cns_adc_temperature_measurement

Overview

The adc_temperature_measurement examples shows how to measure internal temperature sensor.

By selecting internal voltage reference 1.2V, 16-bit audio ADC accuracy and by measuring the internal temperature sensor, the temperature is calculated according to the following formula: Tmeans(in C) = Conversion Result/TS_GAIN - TS_OFFSET.

Supported Boards