This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

cadc_continuous_dma_conversion

Overview

The CADC continuous DMA demo application demonstrates the usage of the ADC and DMA peripheral while in a Loop Sequential mode. The CADC is first set to Loop Sequential mode. In Loop Sequential convert configuration, only the initial rising-edge to launch continuous conversions is observed, and until conversion is aborted, the CADC continues to do conversions on the same CLIST register that initiated the conversion. DMA request will be asserted during an CADC conversion READY event noted when any of the ADC_RDY[RDYn] flags is asserted. DMA will transfer CADC results to memory and if users press any key, demo will average CADC results stored in memory and print average on the terminal.

Supported Boards