This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

edma_address_offset

Overview

The EDMA address offset example is a simple demonstration program that uses the SDK software. It excuates a simple transfer from source buffer to destination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the EDMA minor loop/major loop offset feature and to provide a simple example for debugging and further development. Note: The examples is also trying to show when minor loop offset and major loop offset are both enabled for a channel, the last minor loop offset will not applied to address and the major loop offset will applied to the address.

Supported Boards