This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexcan_loopback_edma_transfer

Overview

The flexcan_loopback_edma example shows how to use the EDMA version transactional driver to receive CAN Message from Rx FIFO:

To demonstrates this example, only one board is needed. The example will config one FlexCAN Message Buffer to Tx Message Buffer and also setup Rx FIFO. After that, the example will send 4 CAN Messages from Tx Message Buffer to Rx FIFO through internal loopback interconnect and read them out using EDMA version FlexCAN transactional driver. The Sent and received message will be print out to terminal at last.