This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dsc_lpi2c_interrupt

Overview

The lpi2c_interrupt example shows how to use lpi2c driver as master and slave to do 2 lpi2c instance for internal transfer with interrupt:

In this example, one lpi2c instance as master and another lpi2c instance as slave. Master sends a piece of data to slave, and receive a piece of data from slave.

Supported Boards