This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dspi_polling_transfer

Overview

The dspi_polling_transfer example shows how to use DSPI driver in polling way:

In this example , one dspi instance used as DSPI master and another dspi instance used as DSPI slave in the same board.

  1. DSPI master send/received data to/from DSPI slave in polling . (DSPI Slave using interrupt to receive/send the data)