This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

edma4_interleave_transfer

Overview

The EDMA interleave transfer example is a simple demonstration program that uses the SDK software. It excuates interleave transfer from source buffer to destination buffer using the SDK EDMA drivers. The purpose of this example is to show how to use the interleave feature of EDMA and to provide a simple example for debugging and further development. The example demostrates the interleave transfer by features:

Supported Boards