This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

elcdif_lut

Overview

The ELCDIF LUT project shows how to use the ELCDIF LUT to convert 8-bit input pixel to 24-bit output pixel. There are two LUT memories, this project uses one input frame buffer, and swithes between the two memories, so from the LCD panel, two different pictures are shown one by one.

Supported Boards