This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

enet_txrx_transfer

Overview

The enet_rxtx example shows the simplest way to use ENET driver for simple frame receive and transmit.

  1. This example shows how to initialize the ENET MAC.

  2. How to use ENET MAC to receive and transmit frame.

The example transmits 20 number broadcast frame, print the frame length, source MAC address and destination MAC address when receive frame.

Note, The RMII mode is used for default setting to initialize the ENET interface between MAC and the external PHY. you can change it to MII mode as you wish. Please make sure the MII Mode setting in the MAC is synchronize to the setting in TWR-SERIAL board for the external PHY.

Supported Boards