This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

eeprom_ftmr

Overview

The EEprom example shows how to use flash driver to operate program EEprom:

Running the demo

When the example runs successfully, you can see the similar information from the terminal as below.

EEprom example Start

EEprom Information: Total EEprom Size: xx KB, Hex: (xx) EEprom Sector Size: xx B, hex: (xx) Erase eight sector of EEprom Program a buffer to eight sector of EEprom Successfully Programmed and Verified Location xx -> xx

End of EEprom example

Supported Boards