usart_wakeup_deepsleep
Overview
The usart_wakeup_deepsleep example shows how to use usart driver in 32kHz clocking mode to wake up soc from deep sleep.
In this example, one usart instance is connected to PC, the board will enter into deep sleep mode and wake up according to user input.