This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexio_pin_input_interrupt

Overview

The FLEXIO PIN Example project is a demonstration program that uses the FLEXIO software to manipulate the flexio-pin as input function. The example uses FLEXIO-PIN input to capture the edge of other gpio pin.

Supported Boards