This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexio_uart_interrupt_transfer

Overview

The flexio_uart_interrupt example shows how to use flexio uart driver in interrupt way:

In this example, a flexio simulated uart connect to PC through USB-Serial, the board will send back all characters that PC send to the board. Note: two queued transfer in this example, so please input even number characters.

Supported Boards