This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexspi_hyper_ram_polling_transfer

Overview

The flexspi_hyper_ram_polling_transfer example shows how to use flexspi driver with polling:

In this example, flexspi will send data and operate the external Hyper RAM connected with FLEXSPI. Some simple flash command will be executed, such as Read ID, Read Data and Write Data. Example will first Write 256 bytes of data from the start of Hyper ram, then read the data back. at last check if the data in flash is correct.

Supported Boards