This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexspi_nor_dma_transfer

Overview

The flexspi_nor_dma_transfer example shows how to use flexspi driver with dma:

In this example, flexspi will send data and operate the external nor flash connected with FLEXSPI. Some simple flash command will be executed, such as Write Enable, Erase sector, Program page. Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.

Supported Boards