This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

flexspi_psram_polling_transfer

Overview

The flexspi_psram_polling_transfer example shows how to use flexspi driver with polling:

In this example, flexspi will send data and operate the external PSRAM connected with FLEXSPI. Some simple flash command will be executed, such as Read Data and Write Data. Example will write/read through the whole chip, through IP command and AHB command.

Supported Boards