This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

gdma_transfer_basic

Overview

This project shows how to use GDMA transactional APIs to do the basic memory to memory data transfer. In this example, GDMA copies data from one buffer to another buffer, when copy finished, the two buffer content are compared to make sure the transfer succeed. The compare result is shown in the terminal.

Supported Boards