This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

gpt_capture

Overview

The gpt_capture project is a simple demonstration program of the SDK GPT driver’s input capture feature. The example sets up a GPT channel for rise-edge capture. Once the input signal is received, this example will print the capture value.

Supported Boards