This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

i3c_dma_b2b_transfer_slave

Overview

The example shows how to use i3c driver as slave to do board to board transfer with a DMA master.

In this example, one i3c instance as slave and another i3c instance on the other board as master. Master first sends a piece of data to slave in I2C mode, and receive a piece of data from slave and check if the data received from slave is correct. Then master will enter dynamic address cycle to assign address to the connected slave, after success, will use I3C SDR mode to transfer data, then receive data from the connected I3C slave and check the data consistency.

Supported Boards