This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

iap3_flash

Overview

The IAP flash project is a simple demonstration program of the SDK IAP driver. It provides some flash operations with ROM API, such as automatically detect flash configuration, erase sectors and program pages. All operations are followed by flash memory check to ensure the data operated are successful.

Supported Boards