This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

igpio_input_eqdc_signal

Overview

The GPIO Example project is a program functioning as an encoder which outputs two quadrature signals and one interrupt signal.

The example is supported by the set, clear registers, and toggle write-only registers for each port output data register.

Running the demo

When the example runs successfully, the following message is displayed in the terminal: If you turn on the SW8 , and “SW8 is turned on, INDEX generated” is shown on the terminal window

 GPIO Driver example.

 Out put signals for EQDC module.

 SW8 is turned on, INDEX generated.
 ......

Supported Boards