This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

isi_ci_pi_yuv422

Overview

This example shows how to use ISI to receive camera frame through CI_PI.

In this example, the camera input frame is YUV422 format and ISI output frame is RGB656 format. The output frame is shown in the screen.

NOTE: This example must run continously to get the right result, breaking during debug will results to display tearing. Because the ISI driver maintains IP state through ISR, if the core is halted, then driver state does not match the IP state. When exiting debug, the core might be halted for a short while, so the tearing may happen when exiting debug.

If the camera and LCD panel resolutions are not the same, then only part of the camera frame will be shown.