This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

iuart_auto_baudrate_detect

Overview

The uart_auto_baudrate_detect example shows how to use uart auto baud rate detect feature:

In this example, one uart instance connect to PC through uart. First, we should send characters a or A to board. The boars will set baud rate automatic. After baud rate has set, the board will send back all characters that PC send to the board.

Supported Boards