This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

pwm_output

Overview

The pwm_output project is a simple demonstration program of the SDK PWM driver. The pulse width modulator (PWM) module contains PWM channels, each of which is set up to output different signals. This PWM module can generate various switching patterns, including highly sophisticated waveforms.