This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lcdif_porter_duff

Overview

This example demonstrates how to use the LCDIF alpha blend function to perform the Porter Duff compositing. In this example, a red rectangle of overlay layer 0 is in the top left corner of the panel as source surface, and a blue rectangle of the video/graphic layer is at the bottom right position of the red one as destination surface. Every Porter Duff mode result is shown for 2 seconds, then switch to the next mode.

Supported Boards