This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lcdifv2_lut

Overview

This example demonstrates how to use the LCDIF v2 color palette (LUT). In this example the pixel format is 8-bit LUT index. Although the LUT supports 256 items in this example only items 0-7 are used, because the frame buffer content are restricted to 0-7.

When the example runs, a rectangle is moving in the screen, and its color changes when touch border.

Supported Boards