This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpadc_dma

Overview

The lpadc_dma example shows how to use ADC to trigger a DMA transfer.

In this example, user should indicate a channel to provide a voltage signal (can be controlled by user) as the LPADC’s sample input. When running the project, typing any key into debug console would trigger the conversion, the software trigger API is called to start the conversion. When the ADC conversion is completed, it would trigger the DMA in ping-pong transfer mode to move the ADC conversion result from ADC conversion data register to user indicated memory. Then the main loop waits for the transfer to be done and print the latest ADC conversion word and ADC conversion value average to terminal.

Supported Boards