This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

niobe4analog_flexspi_nor

Overview

The FLASIAP NOR project is a simple demonstration program of the SDK FLASIAP NOR driver. It erases and programs a portion of external Nor flash connected with FLEXSPI. Some simple flash command willbe executed,such as Write Enable, Erase sector, Program page. Example will first erase the sector and program a page into the flash, at last check if the data in flash is correct.

Supported Boards