This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpc_adc_dma

Overview

The lpc_adc_dma example shows how to use LPC ADC driver with DMA.

In this example, the sensor is used to created the input analog signal. When user type in any key from the keyboard, the software trigger API is called to start the conversion. When the ADC conversion is completed, it would trigger the DMA to move the ADC conversion result from ADC conversion data register to user indicated memory. Then the main loop waits for the transfer to be done and print the result to terminal.

Project Information

1.what are ADC conversion sequences? A conversion sequence is a single pass through a series of A/D conversions performed on a selected set of A/D channels. Software can set-up two independent conversion sequences, either of which can be triggered by software or by a transition on one of the hardware triggers. Each sequence can be triggered by a different hardware trigger. One of these conversion sequences is referred to as the A sequence and the other as the B sequence. It is not necessary to employ both sequences. An optional single-step mode allows advancing through the channels of a sequence one at a time on each successive occurrence of a trigger. The user can select whether a trigger on the B sequence can interrupt an already-in-progress A sequence. The B sequence, however, can never be interrupted by an A trigger.

  1. How to use software-triggered conversion? There are two ways that software can trigger a conversion sequence:

    1. Start Bit: The first way to software-trigger an sequence is by setting the START bit in the corresponding SEQn_CTRL register. The response to this is identical to occurrence of a hardware trigger on that sequence. Specifically, one cycle of conversions through that conversion sequence will be immediately triggered except as indicated above. (In this example, we use this way.)

    2. Burst Mode: The other way to initiate conversions is to set the BURST bit in the SEQn_CTRL register. As long as this bit is 1 the designated conversion sequence will be continuously and repetitively cycled through. Any new software or hardware trigger on this sequence will be ignored.

  2. How to use DMA to work with ADC? The sequence-A or sequence-B conversion/sequence-complete interrupts may also be used to generate a DMA trigger. To trigger a DMA transfer, the same conditions must be met as the conditions for generating an interrupt. Remark: If the DMA is used, the ADC interrupt must be disabled in the NVIC.

Program Flow

1.This example demonstrates how to configure the A sequences with interrupt, assigning one channel with software trigger, you can configure channel via “DEMO_ADC_SAMPLE_CHANNEL_NUMBER”.

2.Before configuration of the ADC begins, the ADC is put through a self-calibration cycle.

3.Configure the DMA and DMAMUX to work with ADC sequences.

4.Enable the Conversion-Complete or Sequence-Complete DMA for sequences A.

5.After ADC channels are assigned to each of the sequences, if the user enters any key via terminal, software trigger will start.

6.When the conversion completes, the DMA would be requested.

7.When the DMA transfer completes, DMA will trigger a interrupt. ISR would set the “bDmaTransferDone” to ‘true’. Then main function will print conversion result to terminal.

Supported Boards