This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

dma_hardware_trigger

Overview

The DMA hardware trigger example is a simple demonstration program that uses the SDK software.It executes one shot transfer from source buffer to destination buffer using the SDK DMA drivers by hardware trigger.The purpose of this example is to show how to use the DMA and to provide a simple example fordebugging and further development.

Supported Boards