This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpc_gpio_input_interrupt

Overview

The GPIO input interrupt example is a demonstration program that uses the KSDK software to manipulate the general-purpose GPIO input interrupt. The example is supported to set with selection of polarity and edge vs level triggering and all GPIO pins can optionally contribute to one of two GPIO interrupts.

Supported Boards