This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

i2c_interrupt_transfer

Overview

The I2C Example project is a demonstration program that uses the KSDK software transfer data over Inter-Integrated Circuit interface. The example uses the one i2c instance as the master to send data to another i2c instance as the slave. The slave checks the data it receives and shows the log.