This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

spi_polling_transfer_slave

Overview

The spi_polling_transfer_slave example shows how to use spi driver as slave to receive data from master.

In this example, one spi instance as slave and another spi instance on other board as master. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from master is correct. This example should work with spi_polling_transfer_master example. And this example should start first.