This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

spi_half_duplex_polling_master

Overview

The lpc_spi_half_duplex_polling_transfer_master example shows how to use driver API to transfer in half-duplex way.

In this example, one spi instance as master and another spi instance on the othere board as slave. Master sends a piece of data to slave, and receive a piece of data from slave. This example checks if the data received from slave is correct. Besides, master will transfer data in polling way.