This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

usart_interrupt_rb_transfer

Overview

The uart_interrupt_ring_buffer example shows how to use uart driver in interrupt way with RX ring buffer enabled:

In this example, one uart instance connect to PC through uart, the board will send back all characters that PC send to the board.

Note: The example echo every 8 characters, so input 8 characters every time.