This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpi2c_polling_transfer

Overview

The LPI2C Example project is a demonstration program that uses the KSDK software to manipulate the Low Power Inter-Integrated Circuit. The example uses one lpi2c instance as the master to send data to another lpi2c instance as the slave. The slave will check the data it receives and shows the log.