This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

lpspi_qspi_flash

Overview

This example shows how to use LPSPI to control the QSPI flash, such as erasing, programing, reading. To simplify the code, this example uses GPIO to control the PCS, but not use LPSPI to control it.

When the project run finished, you can see the pass or fail information from the terminal.

Supported Boards