This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mcan_loopback

Overview

The mcan_loopback example shows how to use the loopback test mode to debug your CAN Bus design:

To demonstrate this example, only one board is needed. The example will config Tx Buffer to send and Rx Fifo to receive. After that, the example will send a CAN Message throuth internal loopback interconnect and print out the Message payload to the terminal.

Supported Boards