This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mu_interrupt

Overview

The mu_interrupt example shows how to use MU driver in interrupt way:

In this example:

  1. Core 0 send message to Core 1 in interrupt mode via MU module.

  2. Core 1 send message back to Core 0 in interrupt mode.

  3. Core 0 receive message sent from Core 1 in interrupt mode.

Supported Boards