This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

netc_psi_vsi_message

Overview

The Multicore NETC PSI-VSI demo application demonstrates how to set up projects for individual cores on a multicore system. In this demo, the primary core use NETC PSI to send/receive frames. It also releases the secondary core from the reset. The secondary core toggles an on-board LED indicating that the secondary core is running and uses NETC VSI to send/receive frames.

Supported Boards