This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

mcx_opamp_basic

Overview

The OPAMP basic example demonstrates how to use the OPAMP driver. In this example, the OPAMP works in the internal gain mode, connect the positive terminal of the OPAMP to the external input source. The OPAMP output is 2X of the external input voltage. When the input voltage changes, the OPAMP output changes accordingly.

Supported Boards