This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

opamp_fast_lpadc

Overview

The OPAMP lpadc example demonstrates how to use the OPAMP driver. In this example, the reference voltage (Vref) of the OPAMP1 non-inverting input port comes from the output port of OPAMP0, which needs to be connected to an LPADC channel, the OPAMP1 non-inverting input port needs to be connected to a voltage source and an LPADC channel, the OPAMP1 inverting input port needs to be connected to GND, and the OPAMP1 output port needs to be connected to an LPADC channel.

When this example runs successfully, the terminal will print the OPAMP0 output port voltage value, the OPAMP1 non-inverting input port voltage value, the OPAMP1 output voltage value measured using lpadc, and the theoretical OPAMP1 output value.

The theoretical calculated value should be very close to the value measured by LPADC.

OPAMP1 input and output relationship formula: Vout = Vref + (R2 / R1 * (Vp - Vn)).

Supported Boards