This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

otfad_keyblob

Overview

The OTFAD example shows how to use on the fly AES-128 decryption driver.

In this example, the external flash memory will be used to show the example. The flash memory will store ciphertext and keyblob, and this example will use OTFAD to decrypt ciphertext with flexspi. The FlexSPI fetches the context 0 key blob from the external flash memory, sends the data to the OTFAD which automatically performs the required key blob unwrap function and loads the recovered plaintext data into the context 0 programming model registers. OTFAD always processes key blob data for all four contexts when enabled, and the flash A1 zero address has been loaded valid key wraped data for all four contexts and OTFAD will decryption automatically.

Supported Boards