This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

hostif_spi

Overview

This example shows how to use hostif driver as slave to do board to board transfer with interrupt:

In this example, one spi instance as slave and another spi instance on the host board as master. Master sends a piece of data to slave, and receive a piece of data from slave.