This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

rtc_freerunning

Overview

The RTC project is a simple demonstration program of the SDK RTC driver. The test will set the RTC free running interrupt threshold to be the 32K value and free running interrupt will occur every one second.