This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

queued_spi_edma_b2b_transfer_master

Overview

The queued_spi_edma_b2b_transfer example shows how to use QUEUEDSPI driver in edma way:

In this example, we need two boards, one board is used as QUEUEDSPI master and the other board is used as QUEUEDSPI slave. The file ‘queued_spi_edma_b2b_transfer_master.c’ includes the QUEUEDSPI master code.

  1. QUEUEDSPI master sends/receives data to/from QUEUEDSPI slave in edma way. (QUEUEDSPI Slave uses edma way to receive/send the data)

Supported Boards