This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

queued_spi_polling_b2b_transfer_slave

Overview

The queued_spi_polling_b2b_transfer example shows how to use QUEUEDSPI driver in polling way:

In this example we need two boards, one board is used as QUEUEDSPI master and another board is used as QUEUEDSPI slave. The file ‘queued_spi_polling_b2b_transfer_slave.c’ includes the QUEUEDSPI slave code.

  1. QUEUEDSPI master sends/receives data to/from QUEUEDSPI slave in polling. (QUEUEDSPI Slave uses interrupt to receive/send the data)

Supported Boards