This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

adc_interrupt

Overview

The SAR ADC interrupt example shows the simplest way to use the SAR ADC driver.

In this example, three channels (channels 0, 1, and 2) are used to form a conversion chain, these three channels are executed in the normal conversion scan mode. The end-of-channel interrupt, pre-sample, DMA transfer and watchdog features of each channel in the conversion chain are disabled, and the end-of-chain interrupt is enabled. The user should provide a voltage signal as input to each conversion channel. When running the project, type any key into the debug console to get these three channels’ conversion result, when the conversions in the chain are completed, the end-of-chain interrupt will be triggered, and if the result of channel conversion is valid, it will be printed to the debug console.

Supported Boards