This is the documentation for the latest (main) development branch of mcuxpresso sdk. If you are looking for the documentation of previous releases, use the drop-down menu on the left and select the desired version.

sctimer_simple_pwm

Overview

The SCTimer project is a simple demonstration program of the SDK SCTimer’s driver capabiltiy to generate PWM signals. The SCTimer project enables a 32-bit counter to output two center-aligned PWM signals with parameters set to 24kHz frequency. The duty cycles of the two PWM signals are 50% and 20%, respectively.

Supported Boards